Technical FAQs

Ask a Question

What are the basic components to be ordered for communication of Compact NSX MCCB.

The basic components to be ordered for communication of Compact NSX MCCB are given below
 
a)                  Modbus communication interface module – TRV00210
b)                  NSX cord - It is available in different length sizes                        
            NSX cord L = 0.35 m - LV434200
            NSX cord L = 1.3 m - LV434201
            NSX cord L = 3 m - LV434202 
            NSX cord for U > 480 V AC L = 1.3 m - LV434204
 
c)        BSCM module    LV434205
Was this helpful?
What can we do to improve the information ?