Technical FAQs

Ask a Question

What is the ordering reference of Masterpact NW ACB 220V AC gear motor.

The ordering ref. of Masterpact NW ACB 220V AC gear motor is 47894 (200/240VAC ).
 
 Also, we have to order terminal block which depends upon the type of ACB (manual/drawout).
           
 For Fixed circuit breaker – 47074
 For Drawout circuit breaker – 47849
 
Was this helpful?
What can we do to improve the information ?