Technical FAQs

Ask a Question

What are the ordering references of spreaders and phase barriers of Simpact MCCB to be ordered as a spare.

         For Frame Size T1
 
            NKS100R, NKS160R, NKS200R, NKF100D       
                     
 
            Spreaders (3P)                                                                          NKSP13
 
           For Frame Size T2
 
           NKF250D 3P/4, NKF100C/K 3/4P, NKF250C/K 3/4P
 
           Spreaders (3P)                                                                           NKSP33
 
           Spreaders (4P)                                                                           NKSP44

         Note : The phase barriers for Simpact MCCB upto 250A will come along with the spreaders as a 
                     default & can’t be ordered as a spare.

          For Frame Size T3
 
          NKF400C/K, NKF400C/K 3/4P        
     
          We do not offer spreaders & phase barriers for frame size T3 of Simpact MCCB as a spare.
 
Was this helpful?
What can we do to improve the information ?