Technical FAQs

Ask a Question

Is Line Load reversibility available in Compact CVS & Simpact MCCB.

The Line or load can be connected to either side of the Compact CVS and Simpact MCCB without any reduction in performance.
Was this helpful?
What can we do to improve the information ?