Technical FAQs

Ask a Question

Do we have MCCB in our range for 400 Hz application.

We have Compact NSX MCCB in our range that can be used for 400 Hz application with a max. breaking capacity “Icu” of 10 kA.
Due to the higher frequency, circuit breakers are subjected to additional temperature rise for identical current levels, resulting from
higher losses caused by Foucault currents and an increase in the skin effect (reduction in the useful CSA of conductors).
To remain within the rated temperature-rise limits of devices, current derating is required.The power levels of 400 Hz applications
rarely exceed a few hundred kW with relatively low short-circuit currents, generally not exceeding four times the rated current.
Please find the below chart for the derating factor for Thermal & Magnetic trip units.

Was this helpful?
What can we do to improve the information ?