Technical FAQs

Ask a Question

Do we have any Type 2 coordination chart for DOL & Star-Delta motor starters operational voltage of 220/240 V AC, 500/525 V AC & 690 V AC.

The Type 2 coordination chart for DOL & Star-Delta motor starters at an operational voltage of 220/240 V AC, 500/525 V AC & 690 V AC is available.
Please refer the below attached file.
Note: In case of Star-Delta starters , please order 3 No.’s of contactors as per the power rating of motor.
 

Was this helpful?
What can we do to improve the information ?