Technical FAQs

Ask a Question

What type of EEPROM Catridges are available for Twido Controllers.

Below mentioned EEPROM (Electrically Erasable Programmable Read-Only Memory)Catridges are available for Twido Controllers:
 
1.TWDXCPMFK32 (32KB MemoryEEPROM Catridge for all compact base controllers for application backup and program transfer).
 
2.TWDXCPMFK64 (64KB Memory EEPROM Catridge for compact base controllers TWDLCAA40DRF,TWDLCDA40DRF,TWDLCAE40DRF,
   TWDLCDE40DRF for memory expansion,application backup and program transfer).
 
Was this helpful?
What can we do to improve the information ?