Technical FAQs

Ask a Question

Can TwidoPort Module 499TWD01100 connected to Twido Controller act as Master on Modbus TCP/IP network.

TwidoPort Module 499TWD01100 when connected to Twido Base controller like TWDLCAA24DRF will always act as 
Slave on Modbus TCP/IP network while communicating to a Master PLC (Programmable Logic Controller) with
embedded Ethernet Port like Twido Compact Controller TWDLCAE40DRF OR Modicon M340 Processor BMXP342030.
Was this helpful?
What can we do to improve the information ?