Technical FAQs

Ask a Question

What is CANJ1939 Protocol and does Schneider have any controller that support CANJ1939.

From Schneider Electric Range,only Twido Extreme Base controller TWDLEDCK1 supports CANJ1939 Protocol.
 
CANJ1939 is a protocol for automobile applications allowing communication with engines.
 
Refer to attached document for information on CANJ1939 Protocol.
Was this helpful?
What can we do to improve the information ?