Technical FAQs

Ask a Question

What is the significance of the LABL in the setup table of DigitAN EM 6400.

The user can set the LABL as 123, AbC, rSt, Pqr and ryb, depending on the country and the requirement.
These labeling options are to satisfy the international standards or requirements. In India normally people use ryb.
These are used for identifying the phase wise parameters.
 Example:
If 123 is selected as label, then the phase wise current will be displayed as A1, A2, A3. 
If ryb is selected as label, then the phase wise current will be displayed as Ar, Ay, Ab. 
Was this helpful?
What can we do to improve the information ?