Technical FAQs

Ask a Question

What is the significance of I.d in DigitAN EM 6400.

This is a unique address called unit id, which is required for identifying the meter while communicating through
 RS 485 port. Unit id is editable from 001 to 255 through the meter set up. 
Was this helpful?
What can we do to improve the information ?