Technical FAQs

Ask a Question

What is SIM mode and why it is required in DigitAN EM 6400 meter.

Simulation mode is provided for the purpose of demonstration of the features of the meter and in exhibition displays.
In this mode user can see the functioning of the meter without any input signals, meter shows fixed Frequency, voltage and
current and 0.5PF. Power and Energy parameters calculated based on this V (240VLN), A (5000A) and PF (-0.5) are displayed.
Was this helpful?
What can we do to improve the information ?