Technical FAQs

Ask a Question

How to set Modicon M258/LMC058 Controller to RUN mode after program download using USB.

It is possible to set Modicon M258/LMC058 Controller to RUN mode automatically after program download
using USB cable with SoMachine V3.0 as per attached document.
Was this helpful?
What can we do to improve the information ?