Technical FAQs

Ask a Question

Is there any option for the fixed type NW10 HA10 circuit breaker as it is only available in draw-out type.

This offer NW10 HA10 is limited to draw-out circuit breaker and rear connection. There is no offer for the fixed or front connection
due to breaking constraint (less performance and need to increase the safety perameter), as this offer is for the 1150V application.
Was this helpful?
What can we do to improve the information ?