Technical FAQs

Ask a Question

What is the material used in Compact NSX connection terminals.

The material used in the Compact NSX terminal connectors is as below:
 
1. Compact NSX100-250 : Copper (Cu) + Tin coating
 
2. Compact NSX 400-630: Copper (Cu) + Silver (Ag) coating
Was this helpful?
What can we do to improve the information ?