Technical FAQs

Ask a Question

Does Compact NS/NSX Switch Disconnector (NA) have the Reflex Tripping feature.

Yes, Reflex Tripping is available in all Compact NS/NSX Switch Disconnectors.The threshold of the Reflex Tripping auto-protection is
about 20xIn and time delay is less than 10 ms. The Reflex Tripping is due to "Piston - which is purely mechanical” and not due to the trip unit.

Thus the Reflex Tripping being a mechanical controlled function is also available in the Compact NS/NSX Switch Disconnectors.
Was this helpful?
What can we do to improve the information ?