Technical FAQs

Ask a Question

What is the value read by the Micrologic trip unit if the Ir setting is done in between of the two setting.

 Regarding the LR plug settings in Micrologic trip unit, if the knob is between two positions the trip unit takes into
 consideration the last valid setting.
 For example, If the setting on 0.98 and we move between 0.98 and 1, the position is kept at 0.98. On the other
 hand, if we move from 1 to between 1 and 0.98 the setting is kept at 1.
Was this helpful?
What can we do to improve the information ?