Technical FAQs

Ask a Question

Double word or floating point values do not display correctly on an XBTGT, HMISTO, or HMISTU HMI.


If a double word or floating point variable from a PLC displays incorrectly on an XBTGT, HMISTO, or HMISTU HMI, it may be that the double word order is set the wrong way round.  By default, Vijeo designer sets the high byte first.  If Premium, Micro, M340, or Twido processors are used, the word order should be changed to ‘Low byte’ first.
 
To change this, in the Vijeo designer navigator pane, double click on the appropriate network under ‘IO manager’ and then select ‘Low byte first’ in the ‘Double word’ order options.
 
Build and save the project then download it to the HMI, the display should then show the double word or floating point value correctly.


 
Was this helpful?
What can we do to improve the information ?