Technical FAQs

Ask a Question

Can we offer Masterpact NW 4000A with Micrologic 7.

Micrologic 7 can be offered up to 3200A for Masterpact NW ACBs because the highest rating of the current available with
the rectangular sensor used with micrologic 7.0 is about 3200A , so we don’t offer 4000A with Micrologic 7.0.
Was this helpful?
What can we do to improve the information ?