Technical FAQs

Ask a Question

What is the meaning of glowing of Ap LED in Micrologic control units.

This is the auto-protection function of the control unit ( excessive temperature or short-circuit higher than circuit-breaker capacity)
which opens the circuit breaker and turns on the Ap LED.
Was this helpful?
What can we do to improve the information ?