Technical FAQs

Ask a Question

Do we have Plug & Sockets available in degree of protection of IP 54 & 55.

We have PK Pratika range of Plug & Sockets available in degree of protection of IP 44, 65 & 67 for current
ratings of  16A , 32 A, 63 A & 125 A.
Was this helpful?
What can we do to improve the information ?