Technical FAQs

Ask a Question

Do we have auxiliary contact blocks available for Capacity duty contactors.

We have in–built instantaneous auxillary contact blocks available in our capacity duty contactors.There is no separate
accessory available for the Capacitor switching contactor". (Eg: LC1DFK11, LC1DLK11 & LC1DTK12 etc.)
You can add a side mounting contact block type LAD8N**. This will provide you with 2 Additional Auxiliary contacts.
However, if you wish to increase the auxiliary contacts further, then use an Auxiliary contactor type CAD32 /CAD50 in
conjunction with the Main Contactor.

There is no possibility to install the front auxiliary contacts type LADN*** on the LC1D*K*** contactor.

Was this helpful?
What can we do to improve the information ?