Technical FAQs

Ask a Question

Which function do user need to capture the SoftMotion Encoder position.

To perform a distance capture on SoftMotion_Encoder:
 
1.In the SoftMotion Encoder Configuration window, choose between falling or rising edge for your two
cap inputs ( For Example-
CAP0: I1.6 and CAP1: I3.6)
 
2.Use MC_TouchProbe to enable and get your distance value.
 
3.With a trigger input= 2,TouchProbe will give you the distance between the two captures. MC_TouchProbe
stays in Busy state until the second capture is done
 
4.In the case described above,I1.6 signal must occur before I3.6. I3.6 will be ignored if CAP0(I1.6) is not already done.
Was this helpful?
What can we do to improve the information ?