Technical FAQs

Ask a Question

Why user must have the administrator right to run SoMachine .What can the user do in order to run SoMachine without of admin rights.

SoMachine needs to read/write files on the C:\Program Files\.... during the runtime. To have access to these
files the user needs to be logged on as administrator.
If user installs SoMachine into another path (not the default path but D:\SoMachine\...for example),it should be
possible to run SoMachine without admin-rights, but this is not recommended by Research and Development Team
as user would get new trouble especially with VijeoDesigner.
Running SoMachine without administrator -rights is neither tested nor validated.
Was this helpful?
What can we do to improve the information ?