Technical FAQs

Ask a Question

What is meaning of error while connecting to Modicon LMC058 Controller "Selected Target system mismatch with the connected device":ID mismatch requested=101a 0219, online=101a 0217 ".Please check in

When user tries to connect PC(PersonalComputer) to LMC058 Controller, the meaning of error
"Selected Target system mismatch with the connected device":ID mismatch requested=101a 0219,online=101a 0217"
signifies that user has configured "101a 0219" in the project by selecting the reference LMC058LF42 (without S0),but
online connected controller to user PC is the "101a 0217" which is LMC058LF42S0.
Was this helpful?
What can we do to improve the information ?