Technical FAQs

Ask a Question

Is it possible to transfer licenses for SoMachine and Solution Extension.Because in the SoMachine registration tool there is nothing about license transfer to another PC.

At the moment,it is not possible to transfer the SoMachine and Solution Extensions licenses using License Manager.
It has to be done by calling to the Registration hotline.
Users have to call the Registration Brick Hotline and they will
request the serial number and more information and user will get an Authorization Code.
 
It is always  possible via phone call,as the Registry Brick team know exactly who has registered SoMachine,where, when,and
whether it is already used or not.

Was this helpful?
What can we do to improve the information ?