Technical FAQs

Ask a Question

Why Modicon M258 Controller shows exception error using 500 characters for CONCAT instruction.

The CONCAT Function block  in SoMachine Software is working only with 255 characters for STRING format.
That is why, user will ways face Exception error for Modicon M258 Controller in SoMachine.
Refer to attached document.
Was this helpful?
What can we do to improve the information ?