Technical FAQs

Ask a Question

How to implement Function Block "ModbusSerialSlave" in SoMachine.

These function blocks and this library will be implicitly used by SoMachine when user is configuring
specific Modbus communication.
For example, if user insert a Modbus IO Scanner,then the library
"IoDrvModbusSerial" is added to the project, because it is using functions from this library.
 
Refer to attached Modbus Serial Document.
Was this helpful?
What can we do to improve the information ?