Technical FAQs

Ask a Question

How do we use G code file with SoMachine.

 Refer to Somachine Project using G Code.
(CNC Application using Modicon LMC058 Controller).
Short Description to use Program Example
1.The program has been made with SoMachine version V2.0RL1.
2.To use the program example,user need only a  Modicon LMC058 Controller.
3.The Lexium 32A Servo Drives are configured in Virtual.
4.The procedure to use this example is:
 Download the program to the LMC058 Controller.
 Export the file "zzz.txt" to the LMC058 Controller.
 With the visualization,start the function "SMC_ReadNCFile".
 With the visualization, start the function "SMC_Interpolator".
Was this helpful?
What can we do to improve the information ?