Technical FAQs

Ask a Question

What are the benefits of selecting “Create project based on starter project” option in the New Project configurations.

When you configure a new project with “Create project based on starter project” selected then it will
automatically creates some of the basic components of the project like :
• Starter page
• Active Alarm page
• Summary Alarm page
• Disabled alarm page
• Hardware alarm page
• Trend page
• Shutdown confirmation
• System Role

As shown below you can choose this option.


Was this helpful?
What can we do to improve the information ?