Technical FAQs

Ask a Question

How to make Vijeo Citect client as a standalone Server.

For your client machines to be worked as separate server you have to set the machine (your system`s) IP address
in the Citect Project Editor >> Server >> Network Address>> In the Address field instead of the Server`s IP address
put your local system`s IP address and replace it. Then go and compile the project. Then go to Tools >> Computer
Setup Wizard >> Select Custom Setup >> Project Name will be appeared then press next >> Then it will show the
Role of your machine as Server And Control Client selected and then confirm it & press next and navigate to the
finish the wizard.After that you can now start your system as a VJC Server.
Was this helpful?
What can we do to improve the information ?