Technical FAQs

Ask a Question

Is it possible to change the IP address of TesysT from LTMCU module.

Yes, you can change or configure the IP address of Tesys T from LTMCU Module.
You have to follow the below process:
 
Go to Configuration mode:-
Services –> config –> Enter config -> Yes
 
 
To Change or Configure Network address go to:-
Services -> Network -> Network settings > Address (set the required address)
 
At the end leave configuration mode by:
Services -> Config -> End config -> Yes
Was this helpful?
What can we do to improve the information ?