Technical FAQs

Ask a Question

What is difference between Portable kits references 34547 and 55391.

The reference 34547 for portable kit is available in Europe and Asia-Pacific countries for ordering
and is set up for supply voltage 220/240VAC.
The reference 55391 portable kit is available for ordering in USA and have the modification as per
the American Voltage standards and is set up for supply voltage 120VAC.
Was this helpful?
What can we do to improve the information ?