Technical FAQs

Ask a Question

What is noise level of motor operation of Motor mechanism for Compact NS<630 MCCB.

The Motor operation MT100 for Compact NS MCCB has a below level of noise during the opening operation.
 
For a ambient noise of 50DBA, the noise level is:
 
- 100DBA at 10cm from the front cover of the product.
- 80DBA at 1meter from the front cover of the product.
 
The Noise level of motor operation of motor mechanism for Compact<630 MCCB is less then the above data.
Was this helpful?
What can we do to improve the information ?