Technical FAQs

Ask a Question

What is the maximum value that the energy counters counts from Sepam 40 and 80 overloads.

The active or reactive energy counters have a metering capacity of 0 to 2.1 x 10 exp8 MWh or Mvarh.
 
When this highest value is reached, the counter start again with 0 value.
Was this helpful?
What can we do to improve the information ?