Technical FAQs

Ask a Question

Is Unity Pro compatible to Windows 7 SP1 (32-bit and 64-bit) operating systems.

Yes Unity Pro V6.0 is compatible to Windows 7 SP1 (32-bit and 64-bit) operating system.
To run Unity Pro 6.0 on Windows 7 64bits System, installation of Windows 7 Service Pack 1 (SP1) is mandatory.
Was this helpful?
What can we do to improve the information ?