Technical FAQs

Ask a Question

Can shockwave file or flash file be played on XBTGT runtime.

No currently shockwave file or flash file can not be played in XBTGT runtime.
Only the supported files that can be played in Runtime are .avi, .mpeg, .mpg, .m1v, .mp2, .vmg or .mp4*2.
Was this helpful?
What can we do to improve the information ?