Technical FAQs

Ask a Question

How many Hardware Dongle can be connected to Vijeo Citect Machine at a time.

Only one Hardware Dongle can be connected to Vijeo Citect Machine at a time.If you want to add-on license feature
on the running Machine the only option is to add those feature in the currently running Hardware Dongle by updating
it with a new authorization code.
 
Was this helpful?
What can we do to improve the information ?