Technical FAQs

Ask a Question

At what temperature do the Altistart 48 fans turn on and off.

 
- Fan Start for a heatsink temperature > 50°C
- Fan Stop for a heatsink temperature < 40°C
Was this helpful?
What can we do to improve the information ?