Technical FAQs

Ask a Question

Do you have any offer of Pushbuttons which can be DIN Rail Mounted.

Yes,Harmony XB4 and XB5 Range Diameter22mm Pushbutton,switches and indicators are generally mounted
on Panel Cut-Outs and Printed Circuit Board Cut-Outs.
However,it is possible to mount Harmony XB4/XB5 Control
and Signalling units on Diameter35mm DIN Rail by using additional Diameter22mm Button Holder Reference 15151 .
 
Refer to attached File for Button Holder Reference 15151.
 
Was this helpful?
What can we do to improve the information ?