Technical FAQs

Ask a Question

Do you have LED brightness information for ZBV Pilot Lights.

Harmony XB4 Range ZBV integral LED series Brightness (Light Intensity)values in terms of mcd(MiliCandela).
 
Colours...... 12V and 24V Supply....48V,120V and 230VSupply
White........  300 mcd....................   270 mcd
Green......... 370 mcd...................  330 mcd
Red............120 mcd....................  110 mcd
Orange....... 170 mcd.................... 150 mcd
Blue...........110 mcd....................  100 mcd
 
NOTE
The higher luminosity at low voltage 12/24V than 48,110 and 230V is due the higher current for these voltages.
Was this helpful?
What can we do to improve the information ?