Technical FAQs

Ask a Question

Do we have rotary handle available for C60 MCBs .

The rotary handle is available for C60, C120, ID RCCB & I switch.
 Rotary handle
 1- Front or lateral control of 2, 3 and 4-pole circuit-breakers.
 2- Degree of protection: IP 40, IK 10.
 A complete rotary handle is made up of a circuit-breaker switching sub-assembly, The references 
are 27046, cat. no. 27047 or cat. no. 27048 as per below specification.

 
Was this helpful?
What can we do to improve the information ?