Technical FAQs

Ask a Question

Do we have horizontal rear connections available for Masterpact NW 6300 A ACB.

In Masterpact NW 6300 A ACB only vertical rear connections are available, there is no horizontal rear
connection available.
Was this helpful?
What can we do to improve the information ?