Technical FAQs

Ask a Question

Will Zelio Soft 2 V4.5 work on Windows 7 64 bit?

Yes, the only current issue that arises is when it comes to communicate between the PC/Laptop and the Zelio Logic Relay, if you use the USB cable SR2USB01 with Windows 7 64 bit version.
However, we have a couple of solutions to overcome this. It will work, if you use one of the following options:
  1. Download the driver for the cable SR2USB01 (for V4.5 running on Windows 7 64bit). Use the following link, download the file that has the driver and a document explaining you how to install it.

  2. Communication between the PC/Laptop and the Zelio Logic Relay using a combination of 2 cables SR2CBL01 (Zelio Relay connector and terminates with serial connector) + SR2CBL06 (converter serial connector to USB connector,CD included will come with drivers for this cable)

    2.   Use the Bluetooth interface SR2BTC01


(If your PC/Laptop doesn’t have Bluetooth already, you can order the Bluetooth adaptor VW3A8115, which will include a CD with the drivers)

    3.   Use the SR2CBL01 cable alone, if your computer/laptop has a serial port available. 

Was this helpful?
What can we do to improve the information ?