Technical FAQs

Ask a Question

How many instances of the DNP3.0 and Modbus/TCP services can be run simultaneously on the BMXNOR0200H module.


When the BMXNOR200H module is configured as a DNP3.0 Server it can support 4 client connections.
When the BMXNOR200H module is configured as a Modbus/TCP Server it can support 16 client connections
Was this helpful?
What can we do to improve the information ?