Technical FAQs

Ask a Question

The MAC ID of the BMX NOE 0100 is 00:80:F4:07:34:9B What is the default IP.

The default IP would be 84.XX.XX.XX where XX are the decimal values of the last three
Octet of the MAC ID so here the Default ID would be 84.07.52.155
Was this helpful?
What can we do to improve the information ?