Technical FAQs

Ask a Question

Is it possible to use the LSU software on standard micrlogic trip unit of compact NSX.

The LSU Software do not works with standard Micrologic in NSX. 
It only works with the demo firmware version of the micrologic for simulation.
The LSU software is only compatible with NSX equipped with Micrologic 5/6.
Was this helpful?
What can we do to improve the information ?