Technical FAQs

Ask a Question

What is the procedure to set up the ENVT Option Setup in 3-Pole compact NSX circuit breaker.

The ENVT option can be set only using RSU through the service tab menu. It is not possible to set this parameter
from the NSX front face trip unit.
Was this helpful?
What can we do to improve the information ?