Technical FAQs

Ask a Question

Can we operate Easypact CVS MCCB in DC networks.

The Easypact CVS with TMD trip unit type F & N for 100/160/250 & 400/630 frame sizes respectively can be used for DC application.

Voltage = 500V/ for 3P
Icu = 15KA(CVS100/160/250)
Icu = 20KA(CVS400/630)

Was this helpful?
What can we do to improve the information ?