Technical FAQs

Ask a Question

Could you explain what the parameter FLC1 means in Tesys T configuration.

FLC1 is used to set the value of nominal current regarding the range of TesysT.
For example if we have a TesysT range 8 amps (LTMR08***) and a motor 2 amps
nominal current we set the FLC1 to 25% because the current of the motor in this
example is the quarter of the full load current here 8amps. When we put 25% in
FLC1 this is means that the current in the register 466 (value of current in percent)
take the value of 100% when you reach 25% of the range of TesysT.

The purpose of  FLC1 is to set the level of current where you are at the nominal
current regarding  the range of the TesysT.
Was this helpful?
What can we do to improve the information ?